Application Notes

:
-or-
:
-or-
:

1 result(s) found.
Number Abstract Type Size
AN-80 v0 Smart-UPS configuration application note
Smart-UPS and Smart-UPS XL behavior can be flexibly adjusted to the actual operating condition through an extended set of user-configurable parameters. Proper parameter setting highly enhances the UPS performance thus considerably increasing reliability and availability of the power protection as a whole. This application note is intended for Smart-UPS and Smart-UPS XL users. The purpose of this note is to help Smart-UPS and Smart-UPS XL users further enhance the quality of power protection by providing a detailed discussion on how to properly adjust Smart-UPS behavior in order for it to deliver the best performance in the particular conditions.
1416 KB