Application Notes

:
-or-
:
-or-
:

9 result(s) found.
Number Abstract Type Size
AN-169 v0 Using PowerChute Network Shutdown in Parallel Redundant or Parallel Capacity UPS Configurations
This Application Note provides an overview of Parallel-UPS configurations and explains the PowerChute Network Shutdown event handling process for UPS's in these configurations.
176 KB
AN-168 v0 APC Modbus Installation and Troubleshooting for AP9635 Network Management Card
This application note explains how to install the Modbus wiring for an AP9635 Network Management Card, gives an overview of the Modbus protocol, describes the Modbus packet structure, and explains how to identify and resolve common problems.
213 KB
AN-170 v0 PowerChute Network Shutdown Operating Modes and supported UPS Configurations
This Application Note provides an overview of what each UPS configuration supported by PowerChute Network Shutdown entails, which UPS families support each configuration and a summary of UPS Model and UPS Network Management Card compatibility for different configurations.
157 KB
AN-171 v0 Using PowerChute Network Shutdown to protect a NETGEAR® ReadyNAS®
This Application Note explains how PowerChute Network Shutdown integrates with NETGEAR® ReadyNAS® to ensure safe shutdown of your network-attached storage device in the event of an extended power outage.
69 KB
AN-67 v3 APC Network Management Card Security Implementation
This document highlights the industry-standard security implementation on the Network Management Card from Schneider Electric and should be used as a high-level overview of the Network Management Card functionality
441 KB
AN-165 v0 Switched Outlet Groups on SMT and SMX Smart-UPS
Document provides an overview of the application and benifits of the Main and Switched Outlet Groups now available on Smart-UPS SMT and SMX products.
84 KB
AN-101 v2 PowerChute Network Shutdown with more than 50 computers connected to one UPS
This Application Note provides information on the communications mechanism between PowerChute Network Shutdown and the UPS Network Management Card as well as system configuration recommendations if you wish to have more than 50 computers protected by one UPS.
100 KB
AN-20 v3 The Communications Process of PowerChute Network Shutdown
This Application Note describes how the UPS Network Management Card and PowerChute Network Shutdown communicate with each other and outlines some recommended steps to ensure system protection.
110 KB
AN-144 v2 PowerChute Network Shutdown Security Features Overview.
This Application Note provides an overview of the Security features in PowerChute Network Shutdown.
279 KB