Application Notes

:
-or-
:
-or-
:

2 result(s) found.
Number Abstract Type Size
AN-75 v1 Configuring Data Centers to Support HP BladeSystem p-Class Servers
HP BladeSystem p-Class servers operate at a power density 10X higher than that of a typical data center, which demands special attention to the power and cooling system. Success in deploying these servers – there are five basic strategies – requires an understanding of several inputs, including the business needs driving the deployment, user preferences, blade requirements, and constraints. This Application Note considers these inputs, and guides the reader to (1)select the best deployment method from the five basic methods, (2) choose the appropriate rack, cooling, power, and management solutions, and (3) apply these solutions to fit individual needs.
1046 KB
AN-74 v1 Configuration of InfraStruXure for Data Centers to Support Dell PowerEdge 1855 Blade Servers
The Introdcution of blade servers has created many challenges for those who design and support NCPI. InfraStruXure for Data Centers can be configured to meet the dynamic needs of Dell PowerEdge 1855 Blade Servers
297 KB