Application Notes

:
-or-
:
-or-
:

3 result(s) found.
Number Abstract Type Size
AN-169 v0 Using PowerChute Network Shutdown in Parallel Redundant or Parallel Capacity UPS Configurations
This Application Note provides an overview of Parallel-UPS configurations and explains the PowerChute Network Shutdown event handling process for UPS's in these configurations.
176 KB
AN-166 v0 Application of Generators for MGE Galaxy UPS Systems
Document provides an overview of the application of generators for Staic UPS Systems
718 KB
AN-20 v3 The Communications Process of PowerChute Network Shutdown
This Application Note describes how the UPS Network Management Card and PowerChute Network Shutdown communicate with each other and outlines some recommended steps to ensure system protection.
110 KB