Application Notes

View All Application Notes

Special Applications
Branch Offices
Business Continuity
Business Desktop
Cable Network
Cooling
First Time Data Center User
High Density Applications
Home Theater - A/V
Industrial Computers
InfraStruXure
Internet Service Provider & Co-Location Data Centers
Laboratories
Point-of Sale Equipment
Power Over Ethernet (POE)
Power
Racks
Security and Environmental
Server Consolidation
Server Rooms & Data Centers
Servers
Software Management
Storage
Total Facility Protection
VOIP
Wireless LANs (Wi-Fi)
Wiring Closets

Search
Keyword:
-or-
Product Name:
-or-
App Note Number:


8 result(s) found.
Number Abstract Type Size
AN-108 v0 APC Integration with NetApp FAS Series
NetApp has built APC UPS monitoring and safe shutdown into their FAS Series of storage solutions. This application note presents the integration and explains to the user how to configure the UPS monitoring and safe-shutdown feature.
143 KB
AN-88 v0 APC's Integration with AdventNet's ManageEngine OpManager
AdventNet's ManageEngine OpManager is a complete network monitoring software that offers combined WAN, Server and Applications monitoring. This application note explains the integration between APC and AdventNet's OpManager, which enables IT managers to monitor all of their network devices, including SNMP-enabled APC UPSs within the APC InfraStruXure architecture, from one application.
438 KB
AN-85 v0 APC's Integration with Neon Software's LANsurveyor
LANsurveyor is easy to use network and desktop management software that has built-in support for APC's InfraStruXure products. This built-in support provides automatic discovery and mapping of SNMP-enabled APC devices; detailed UPS information; APC device status via SNMP traps and alerts; direct access to web-browser interface of APC devices; and integration with InfraStruXure Manager.
282 KB
AN-106 v1 APC Integration with HP Insight Manager
This app note documents APC’s Uninterruptible Power Supply (UPS) integration with HP's Systems Insight Manager, which was developed by HP and is tested and certified by APC.
152 KB
AN-86 v1 APC Power Protection for Avaya VoIP & IP Telephony Solutions
To ensure high availability all VoIP and IP Telephony systems should have a Uninterruptible Power Supply (UPS) system. APC has a variety of power protection solutions to meet any specific needs for wiring closets, MDFs, server farms or data centers as well as any type of communication devices/endpoints. APC also has in-house availability consulting services who can help customer design and build a high availability power protection infrastructure for their business critical IP Telephony system.
1698 KB
AN-50 v7 APC Power Protection for Cisco VoIP & IP Telephony Solutions
To ensure high availability all VoIP and IP Telephony systems should have a Uninterruptible Power Supply (UPS) system. APC has a variety of power protection solutions to meet any specific needs for wiring closets, MDFs, server farms or data centers as well as any type of communication devices/endpoints. APC also has in-house availability consulting services who can help customer design and build a high availability power protection infrastructure for their business critical IP Telephony system.
1629 KB
AN-30 v4 InfraStruXure Agency Listings
This paper describes the Safety Agency testing and certification that has been done on APC's InfraStruXure line of power and air conditioning products. It explains the thought process behind why a particular standard applies to the product. It also explains the benefits of such testing, in particular when electrical inspectors may have concerns about the acceptability of ISX under local codes. Tables list the various models of power and air products and their corresponding domestic and international safety agency listings.
675 KB
AN-35 v2 Windows Built-in Serial & USB UPS Support
Windows XP is built on Windows 2000’s reliability, but a Personal Computer is only as reliable as its AC power. APC and Microsoft have partnered to include built-in support of Uninterruptible Power Supplies (Battery Backup Systems) in the Windows XP operating system in order to prevent crashes and data corruption due to poor power quality.
467 KB