Application Notes

View All Application Notes

Special Applications
Branch Offices
Business Continuity
Business Desktop
Cable Network
Cooling
First Time Data Center User
High Density Applications
Home Theater - A/V
Industrial Computers
InfraStruXure
Internet Service Provider & Co-Location Data Centers
Laboratories
Point-of Sale Equipment
Power Over Ethernet (POE)
Power
Racks
Security and Environmental
Server Consolidation
Server Rooms & Data Centers
Servers
Software Management
Storage
Total Facility Protection
VOIP
Wireless LANs (Wi-Fi)
Wiring Closets

Search
Keyword:
-or-
Product Name:
-or-
App Note Number:


106 result(s) found.
Number Abstract Type Size
AN-119 v0 InRow RP-CW and InRow RP-DX Environmental Control
The InRow RP controls the environment with four basic functions: cool, reheat, dehumidification, and humidification and various combinations thereof. This application note describes the control process for the InRow RP. In order to provide environmental control, the InRow RP units monitor the temperature and humidity of the return air, temperature and humidity of the supply air, and three remote rack inlet temperatures.
195 KB
AN-142 v0 InRow RC Environmental Control
The function of the InRow RC product is to cool air from the hot aisle and deliver it to the cold aisle at the temperature setpoint. The InRow RC controls the environment with a cooling function only. This document describes the control process for the InRow RC. In order to provide environmental control, the InRow RC unit monitors the temperature of the return air, temperature of the supply air, and a remote rack inlet temperature
134 KB
AN-80 v0 Smart-UPS configuration application note
Smart-UPS and Smart-UPS XL behavior can be flexibly adjusted to the actual operating condition through an extended set of user-configurable parameters. Proper parameter setting highly enhances the UPS performance thus considerably increasing reliability and availability of the power protection as a whole. This application note is intended for Smart-UPS and Smart-UPS XL users. The purpose of this note is to help Smart-UPS and Smart-UPS XL users further enhance the quality of power protection by providing a detailed discussion on how to properly adjust Smart-UPS behavior in order for it to deliver the best performance in the particular conditions.
1416 KB
AN-68 v1 Calculating Power Consumption of FM unit
Provides guidance for proper real power consumption measurement for FM series cooling systems.
42 KB
AN-43 v1 Understanding Delta Conversion Online "Battery Charging" - Part 5
This application note is the fifth in a series that discusses many common misunderstandings about Delta Conversion OnlineTM and also it’s advantages. The subjects of delta conversion, delta transformers, and delta inverter are addressed. Various myths are described and criticized.
190 KB
AN-65 v1 VFD Phase Monitoring Capabilities of the NetworkAIR FM
Explains the means by which NetworkAIR FM monitors and and takes protective action based on input electrical fault conditions
34 KB
AN-14 v1 Call-UPS II Provides Out-of-Band Communications
This note explains how to manage UPS via the telephone lines. The features of Call-UPS II are described, and an application example is described.
112 KB
AN-126 v0 Selection procedure for RC and RP
Describes the procedure for selecting InRow Chilled Water products for successful applications.
81 KB
AN-123 v0 ACRP Remote Air-Cooled Condenser Application and Placement
The InfraStruXure InRow RP (ACRP100, ACRP101, and ACRP102) is an air-cooled DX air conditioner for data centers. All air-cooled air conditioners require the use of remote air-cooled condensers. This application note outlines the placement, refrigerant line pipe sizing, and maintenance of air-cooled condensers for the ACRP100 series units.
97 KB
AN-118 v0 Practices for Pressure Relief Valve Discharge Piping
Many mechanical refrigeration systems containing large quantities of refrigerant possess pressure relief devices. Under certain conditions, these systems are piped to the outdoors to prevent the displacement of air inside a structure. This paper is intended to give a list of best practices for sizing the piping from the discharge of a pressure relief valve to the outside.
110 KB
AN-10 v1 Use of third party proprietary drivers with APC UPSs
APC has been executing on developing management solutions based on industry-accepted standards. Other manufacturers have expended resources in an attempt to utilize a UPS-specific proprietary management package.
115 KB
AN-120 v0 ACRP Requirements for Selecting 3rd Party Remote Air-Cooled Condenser and Flooded Receiver
The InfraStruXure InRow RP (ACRP100, ACRP101, and ACRP102) is an air-cooled DX air conditioner for data centers. All air-cooled air conditioners require the use of remote air-cooled condensers. This application note outlines the requirements for selecting third party remote condenser and flooded receiver for InRow RP air-cooled product.
90 KB
AN-44 v1 Understanding Delta Conversion Online "Input Power Factor Correction" - Part 6
This application note is the sixth in a series that discusses many common misunderstandings about Delta Conversion OnlineTM and also it’s advantages. The subjects of delta conversion, delta transformers, and delta inverter are addressed. Various myths are described and criticized.
205 KB
AN-121 v0 Using MCA and MOP Ratings to Safely Connect Your Field Wired Air Conditioner
The minimum circuit ampacity (MCA) and maximum overcurrent protection (MOP) ratings provide guidance for safely connecting field-wired equipment to the building mains in North America. Understanding these ratings, and their relationship to each other, is critical to properly selecting wire and circuit breaker sizes.
94 KB
AN-132 v0 InRow RC Cooling of HP C-Class Chassis
High performance blade chassis such as the HP c-Class are alleged to be highly problematic regarding thermal solutions within traditional Data Center spaces. APC has developed in row cooling products, such as the InRow RC, to specifically address such challenges.
144 KB
AN-45 v1 Understanding Delta Conversion Online "Output Power Factor Ratings" - Part 7
This application note is the seventh in a series that discusses many common misunderstandings about Delta Conversion OnlineTM and also it’s advantages. The subjects of delta conversion, delta transformers, and delta inverter are addressed. Various myths are described and criticized.
187 KB
AN-108 v0 APC Integration with NetApp FAS Series
NetApp has built APC UPS monitoring and safe shutdown into their FAS Series of storage solutions. This application note presents the integration and explains to the user how to configure the UPS monitoring and safe-shutdown feature.
143 KB
AN-133 v1 Cable Trough, Ladder, and Partition Configuration Guide
Management of power and data cabling is critical for data center installation and long-term maintenance. APC has developed a line of products designed to contain and manage this array of cabling and piping. These products include cable troughs, ladders, and partitions. The following Application Note contains guidelines on positioning these products within a data center, determining cable capacity/fill of each product, planning for location of different services (power, data, cooling) within the data center, and installing these products.
814 KB
AN-131 v0 TUV – Rheinland NRTL Certification
This paper describes use of the TUV-Rheinland NRTL mark in lieu of the UL and C-UL (or CSA) marks for the North American Market (NAM). This paper is limited in scope and should be considered an adjunct to APC Application Note #30, "InfraStruXure Agency Listings".
168 KB
AN-41 v1 Understanding Delta Conversion On-line "DC Bus Power Exchange" - Part 3
This application note is the third in a series that discusses many common misunderstandings about Delta Conversion OnlineTM and also it’s advantages. The subjects of delta conversion, delta transformers, and delta inverter are addressed. Various myths are described and criticized.
201 KB
AN-49 v1 InfraStruXure Battery Safety in the IT Environment - What happens when the ventilation fails
Could the presence of batteries in an IT environment create a fire hazard? The paper examines the cause of some past battery incidents and demonstrates why many layers of safeguards built into the InfraStruXure design are intended to prevent the build-up of hydrogen gas to a dangerous level. Appendices provide examples of gassing calculations in practical applications.
75 KB
AN-128 v0 Data Center Humidification Strategies
ASHRAE recommends maintaining relative humidity in the range of 40-55% at the air inlet of critical data center IT equipment. This application note first considers various methods of quantifying the expected humidification and dehumidification loads for this design humidity range. After determining latent loading, an approach to equipment selection is offered using APC-MGE InRow products; IR-RC, IR-RP and the FM product as an example.
85 KB
AN-27 v1 APC Silcon Battery Breaker/Fuse-box
For Safe and Flexible Operation of APC Silcon Series in an External Battery Configuration
113 KB
AN-151 v1 InfraStruXure RPP Modular Power Distribution Unit: Hot Aisle Containment Application Guidelines and In Row Baying Instructions
The 300-mm Remote Power Panel (RPP) Modular Power Distribution Unit (MPDU) (Only PDPM277H 400V EMEA/APJ/GCN and PDPM144F 208V NAM) is the power source for Rack Mounted Distribution Units and IT loads. As illustrated in Figure 1, it houses the hot-pluggable power backplane, monitoring bus, controller, Web card and the support structure for the Power Distribution Modules. Specially designed offset brackets ship with the unit to allow joining to other InRow® products and racks in the row or in a Hot Aisle Containment System (HACS) configuration. HACS door frame configurations do not allow the 300-mm RPP to be located at the end of the aisle.
343 KB
AN-137 v3 NetShelter SX Cable Management Guidelines
Cable management is an ever increasing concern at the equipment and enclosure level in the data center. The move to higher density servers and switch applications has increased the cable quantity for both data and power. In addition, higher speed data cables are becoming larger in diameter. These factors are pushing the usable space within the enclosure to the limits. Poor cable management causes congestion and restricts airflow. Proper cable management eliminates congestion and allows air to flow unobstructed through the equipment.
543 KB
AN-53 v2 Using APC InfraStruXure Three Phase Whips and RM PDUs for Non-linear Loads
Consulting Engineers and customers frequently express concern about the acceptability of three phase, 4-wire whips and rack-mount PDUs that are used to distribute InfraStruXure power in a nonlinear load environment. APC is frequently challenged to supply 200% rated neutral conductors. APC conducted extensive testing and demonstrated beyond any doubt that the whips and rack-mount PDUs can be safely used in the worst nonlinear load environment. This application note describes the test methods and provides the test results that support that conclusion.
115 KB
AN-40 v1 Understanding Delta Conversion On-line "Power Regulation" - Part 2
This application note is the second in a series that discusses many common misunderstandings about Delta Conversion OnlineTM and also it’s advantages. The subjects of delta conversion, delta transformers, and delta inverter are addressed. Various myths are described and criticized.
330 KB
AN-106 v1 APC Integration with HP Insight Manager
This app note documents APC’s Uninterruptible Power Supply (UPS) integration with HP's Systems Insight Manager, which was developed by HP and is tested and certified by APC.
152 KB
AN-42 v1 Understanding Delta Conversion Online "Power Balance" - Part 4
This application note is the fourth in a series that discusses many common misunderstandings about Delta Conversion OnlineTM and also it’s advantages. The subjects of delta conversion, delta transformers, and delta inverter are addressed. Various myths are described and criticized.
196 KB
AN-12 v1 The APC Computer Interface Port
This application note provides technical information regarding APC UPS computer interface ports. This information is for customers attempting to use the port for unsupported purposes.
137 KB
AN-88 v0 APC's Integration with AdventNet's ManageEngine OpManager
AdventNet's ManageEngine OpManager is a complete network monitoring software that offers combined WAN, Server and Applications monitoring. This application note explains the integration between APC and AdventNet's OpManager, which enables IT managers to monitor all of their network devices, including SNMP-enabled APC UPSs within the APC InfraStruXure architecture, from one application.
438 KB
AN-154 v0 Integrating Physical Threat Monitoring with Surveillance Equipment in Data Center Environments
This application note provides an overview of the integration of the capture, storage, and management functions of a surveillance system with environmental monitoring of physical threats. These functions are typically provided as individual elements within data center environments. Each element alone, while valuable, requires its own management and health monitoring capability. With a common management platform, these elements can be integrated to produce a comprehensive environment and surveillance monitoring system that reduces the total cost of ownership.
309 KB
AN-89 v0 Symmetra MW Features and Benefits
The Symmetra MW modular UPS has gained much recognition in recent years due to its many features and benefits, and strong reliability enhancements over the legacy UPS designs offered by APC’s competition. The focus of this paper is to shed light on some of the many features and benefits compared to that of what other manufacturers in the UPS industry have to offer.
751 KB
AN-20 v2 The Communication Process of PowerChute® Network Shutdown Software
The APC Network Management Card and PowerChute Network Shutdown allow remote shutdown of multiple systems from a single UPS over a network. Awareness of network availability, scalability to large numbers of clients, limited impact on network traffic, and a reliable architecture are of prime concern for such a system. This paper describes how the Network Management Card and PowerChute Network Shutdown communicate with each other to address these concerns.
48 KB
AN-39 v1 Understanding Delta Conversion Online "The Difference" - Part 1
This application note is the first in a series that discusses many common misunderstandings about Delta Conversion OnlineTM and also it’s advantages. The subjects of delta conversion, delta transformers, and delta inverter are addressed. Various myths are described and criticized.
209 KB
AN-81 v1 APC Console Port Servers and Out-of-Band Management for Microsoft Windows® Server 2003
This note provides an overview of out-of-band management, explains Emergency Management Service (EMS), and describes how APC Console Port Servers provide native support for the EMS and the management of Windows Server 2003 server farms, helping to further automate data center management.
144 KB
AN-3 v2 Electrical Site Planning for Matrix
This application note explains how you can prepare for the installation of a Matrix UPS in North America. You will learn what power wiring is needed, and what you will need to do to install the UPS.
71 KB
AN-85 v0 APC's Integration with Neon Software's LANsurveyor
LANsurveyor is easy to use network and desktop management software that has built-in support for APC's InfraStruXure products. This built-in support provides automatic discovery and mapping of SNMP-enabled APC devices; detailed UPS information; APC device status via SNMP traps and alerts; direct access to web-browser interface of APC devices; and integration with InfraStruXure Manager.
282 KB
AN-101 v0 PowerChute® Network Shutdown with more than 50 Computers connected to one UPS
PowerChute® Network Shutdown works with the UPS Network Management Card to provide graceful shutdown of computers powered by a UPS. The number of computers is limited only by the power capacity of the UPS; however, if you wish to have more than 50 computers powered by one UPS, some consideration must be given to the system configuration. Knowledge of the communication between PowerChute and the UPS Network Management Card is necessary.
71 KB
AN-60 v1 Installation of InfraStruXure For Small Data Centers with an Emergency Power Off Circuit
Many installations require the use of and Emergency Power Off (EPO) circuit to disconnect power from a room or apparatus. This requirement was taken into consideration during the design of the APC InfraStruXure architecture. This application note provides guidelines for the installation of InfraStruxure for Small Data Centers with an EPO circuit.
390 KB
AN-102 v0 Communication Options for the APC AV S20 and Home Automation Networks
The APC S Type AV Power Conditioner with Battery Backup is an all-in-one power protection unit that is well suited for high-performance home automation networks and AV systems. This note presents multiple strategies for communication between the APC AV S20 (S20BLK) and home automation networks.
103 KB
AN-149 v0 APC Symmetra® PX 40K UPS Frame Installation Deviation and Selection of Input Circuit Breaker Ratings
The APC Symmetra® PX scalable UPS frames provide customers with unique UPS power level scalability. This document gives the specifications for permitted input circuit breaker sizes for use with the APC Symmetra PX 40K scalable UPS frame and a 208Y/120V, 60 Hz utility source. This Applications Note is applicable to only the following APC SKU’s: SY10K40F , SY20K40F, SY30K40F, SY40K40F, when configured as either standalone systems or with the InfraStruXure® PDU 40kW 208V/208V W/ MBPwD w/o transformer - PDRPPNX10-M. This Applications Note does not apply to any configuration that includes the following APC InfraStruXure® PDU w/ MBPwD SKU’s which include input isolation transformers: PD40F6FK1-M or PD40G6FK1-M or PD40L6FK1-M
269 KB
AN-109 v0 Application Guidelines for the InfraStruXure InRow SC Condenser
The InfraStruXure InRow SC (ACSC100 and ACSC101) is a self-contained air conditioner for server rooms and wiring closets. This application note outlines various considerations for the condenser section to ensure proper operation
222 KB
AN-111 v0 Application Guidelines for the Wiring Closet Ventilation Unit
The Wiring Closet Ventilation Unit (WCVU) is a rapidly deployable wall and ceiling mount heat removal system designed specifically for the wiring closet environment. By exhausting hot air from the closet to an adjacent space, it allows conditioned air to enter the room and cool the load. This application note covers the best practices for deploying the WCVU.
265 KB
AN-50 v7 APC Power Protection for Cisco VoIP & IP Telephony Solutions
To ensure high availability all VoIP and IP Telephony systems should have a Uninterruptible Power Supply (UPS) system. APC has a variety of power protection solutions to meet any specific needs for wiring closets, MDFs, server farms or data centers as well as any type of communication devices/endpoints. APC also has in-house availability consulting services who can help customer design and build a high availability power protection infrastructure for their business critical IP Telephony system.
1629 KB
AN-144 v0 PowerChute Network Shutdown Security Features Overview.
PowerChute Network Shutdown® software works in conjunction with the UPS Network Management Card to provide graceful, unattended shutdown of multiple computer systems over a network. Its scalable architecture can support a virtually unlimited number of client systems. This application note outlines PowerChute Network Shutdown security features for version 2.2.3 and higher.
931 KB
AN-150 v0 APC InfraStruXure® 20kW UPS Installation Deviation and Selection of Input Circuit Breaker Ratings
The APC InfraStruXure® 20kW UPS system provides customers with unique UPS power level scalability. This document gives the specifications for permitted input circuit breaker sizes for use with the APC InfraStruXure® 20kW scalable UPS frame and a 208Y/120V, 60 Hz utility source. This Applications Note is applicable to only the following APC SKU: ISX20K20F.
251 KB
AN-86 v1 APC Power Protection for Avaya VoIP & IP Telephony Solutions
To ensure high availability all VoIP and IP Telephony systems should have a Uninterruptible Power Supply (UPS) system. APC has a variety of power protection solutions to meet any specific needs for wiring closets, MDFs, server farms or data centers as well as any type of communication devices/endpoints. APC also has in-house availability consulting services who can help customer design and build a high availability power protection infrastructure for their business critical IP Telephony system.
1698 KB
AN-147 v1 Proper UPS selection for servers with active PFC power supplies
This document explains why some Back-UPS or Smart-UPS SC models may not be the proper choice for servers and other equipment that use large PFC (power factor corrected) power supplies and/or contain redundant supplies. Active PFC power supplies have become more common on name brand servers to comply with more stringent guidelines for energy consumption. It provides guidance for selecting and properly sizing models that are more suitable for the demands of these applications.
89 KB
AN-47 v1 How APC designs AC power capacitors into large UPS systems
This application note will explain how APC's Silcon and InfraStruXure UPS systems are designed with regard to maximizing the lifetime of its AC power capacitors.
47 KB
AN-28 v3 APC Silcon UPS and Diesel Generator
The APC Silcon UPS has the highest efficiency (AC-AC on-line UPS), at the same time as the input power factor has been regulated to 1, and input current is sinusoidal. This means that APC Silcon has the lowest input power compared to any other UPS systems sold in the market today. In this way it is easy to have APC Silcon operating correctly on a diesel, simultaneously with the very flexible software programming of APC Silcon. At development of the APC Silcon series great efforts have been made as regards control, regulations, as well as optimizing the whole operational mode of the APC Silcon UPS making it completely optimal for operation on a diesel generator
196 KB
AN-75 v1 Configuring Data Centers to Support HP BladeSystem p-Class Servers
HP BladeSystem p-Class servers operate at a power density 10X higher than that of a typical data center, which demands special attention to the power and cooling system. Success in deploying these servers – there are five basic strategies – requires an understanding of several inputs, including the business needs driving the deployment, user preferences, blade requirements, and constraints. This Application Note considers these inputs, and guides the reader to (1)select the best deployment method from the five basic methods, (2) choose the appropriate rack, cooling, power, and management solutions, and (3) apply these solutions to fit individual needs.
1046 KB
AN-72 v0 Cisco approved design specifications : Power and Cooling for Voice Over IP
Joint design specifications on power and cooling requirements for Voice Over IP.
368 KB
AN-83 v0 Facilities Considerations for the Cisco Business Ready Data Center
The Cisco Business Ready Data Center – a comprehensive, adaptive network architecture designed for agile IT support of business needs – critically depends upon underlying physical facilities to provide the power, cooling, physical housing, security, fire protection, and cabling that allow IT to function reliably and seamlessly. This paper presents strategies for designing the integrated, end-to-end facilities that provide this crucial physical infrastructure to support the on-demand computing environment of the Business Ready Data Center.
1213 KB
AN-24 v3 Access Floor Loading for InfraStruXure Type B
This application note provides basic information about access floor (raised floor) loading and what must be done when installing an APC InfraStruXure Type B solution
165 KB
AN-26 v2 EMI and InfraStruXure
InfraStruXure Architechure addresses the potential issue of EMI
55 KB
AN-148 v0 APC Symmetra® PX 80K UPS Frame Installation Deviation and Selection of Input Circuit Breaker Ratings
The APC Symmetra® PX scalable UPS frames provide customers with unique UPS power level scalability. This document gives the specifications for permitted input circuit breaker sizes for use with the APC Symmetra PX 80K scalable UPS frame and a 208Y/120V, 60 Hz utility source. This Applications Note is applicable to only the following APC SKU’s: SY10K80F, SY20K80F, SY30K80F, SY40K80F, SY50K80F, SY60K80F, SY70K80F, and SY80K80F when configured as either standalone systems or with the InfraStruXure® PDU 40kW 208V/208V W/ MBP w/o transformer PDRPPNX14-M. This Applications Note does not apply to any configuration that includes the following APC InfraStruXure® PDU w/MBP SKU’s which include an input isolation transformer: PD80F6FK1-M or PD80G6FK1-M or PD80L6FK1-M.
292 KB
AN-153 v1 Best Practices for Deploying Smart-UPS, Smart-UPS On-Line, and Symmetra
The Smart-UPS, Smart-UPS On-Line, and Symmetra uninterruptible power supplies (UPS) protect hardware, software and data from power disturbances throughout the world. Designed to prevent blackout, brownouts, surges and sags from reaching your IT devices and other valuable electronic equipment, Smart-UPS, Smart-UPS On-Line and Symmetra provide continuous power from its internal battery until the utility line is restored to a safe level. This application note covers best practices for deploying a Smart-UPS, Smart-UPS On-Line or Symmetra as well as environmental constraints.
213 KB
AN-141 v1 RDX Remote Fluid Cooled Condenser ACRP10X
The ACRP10X Series of InRowTM RP cooling products has been designed for use with remote air-cooled condensers, and is supported by a variety of condenser selections from APC. The available condenser selection meets world wide ambient temperature and power supply considerations. While liquid cooled condensers are not directly supported as a factory option, it is a minimal design effort for the installer to select and install an appropriate liquid cooled condenser along with the necessary accessory items. The installation of such a condenser will allow the use of either water or a water / glycol mixture for the heat of rejection medium.
285 KB
AN-76 v2 Configuring Data Centers to Support IBM BladeCenter Servers
The IBM BladeCenter operates at a power density 10X greater than the capability of a typical data center, which demands special attention to the power and cooling system. Success in deploying these servers – there are five basic strategies – requires an understanding of several inputs, including the business needs driving the deployment, user preferences, blade requirements, and constraints. This Application Note considers these inputs, and guides the reader to (1) select the best deployment method from the five basic methods, (2) choose the appropriate rack, cooling, power, and management solutions, and (3) apply these solutions to fit individual needs.
186 KB
AN-30 v4 InfraStruXure Agency Listings
This paper describes the Safety Agency testing and certification that has been done on APC's InfraStruXure line of power and air conditioning products. It explains the thought process behind why a particular standard applies to the product. It also explains the benefits of such testing, in particular when electrical inspectors may have concerns about the acceptability of ISX under local codes. Tables list the various models of power and air products and their corresponding domestic and international safety agency listings.
675 KB
AN-138 v1 Benefits of the Airflow Calculator
Creating optimal data center designs is one of the main priorities for APC, and the following application note outlines the benefits of the real-time calculation of the airflow within a data center design, along with guidelines for optimal layout of data center equipment.
180 KB
AN-140 v1 Bar Code Best Practice
Data centers are constantly changing and new mainstream technologies such as blade servers and virtualization are causing the pace of change to accelerate. One of the tools that can help the data center operators establish processes to manage the rapidly changing environment is bar coding. The following application note offers advice on the various issues to consider prior to introducing bar coding in the data center as well as best practice for successful implementation.
242 KB
AN-110 v1 Cabling Configurations for Analog and IP-based APC KVM Switches
Keyboard Video Mouse (KVM) switches are used worldwide in applications ranging from enterprise data center to small desktop applications and every size application in between. KVM switches are used to consolidate access to computers and servers providing IT administrators with a streamlined management approach. Other benefits include, space savings, decreased hardware costs, and energy savings, by using one monitor, keyboard, and mouse for multiple servers. This paper presents strategies for cascading and daisy-chaining APC KVM Switches.
320 KB
AN-64 v1 InfraStruXure Manager Server Appliance v4.x Security
InfraStruXure Manager is designed with various layers of network and user management security providing a high level of protection from both unauthorised external and internal access to the managed APC devices. InfraStruXure Manager has the ability to incorporate both redundant manageability and dual power sources.
280 KB
AN-93 v1 Security Features of APC's NetBotz Appliances
APC’s NetBotz appliances provide environmental and security monitoring. Many customers have questions concerning the safety and privacy of the data collected by these appliances. This paper outlines the security features of the NetBotz appliances which ensure the security and privacy of the information collected and monitored.
64 KB
AN-32 v1 Application Summary of InfraStruXure in Dell Racks
Provides an application summary for integrating InfraStruXure systems with Dell racks and equipment.
583 KB
AN-92 v0 Best Practices for Designing Data Centers with the InRow RC
The InfraStruXure® InRow RC is designed to provide cooling at the row and rack level of a data center for rack based IT equipment with front to back airflow. When designing data centers with this product, there are some best practices that should be followed to ensure the InRow RC is cooling as designed. This paper presents the best practices that should be followed when designing a data center with the InRow RC, and provides some additional guidelines to follow when some of these best practices can not be adopted as part of the data center layout.
1187 KB
AN-114 v0 Guidelines for Using Rack Air Containment System with InfraStruXure InRow SC
The InfraStruXure® InRow™ SC (ACSC100 and ACSC101) is a self-contained air conditioner for server rooms and wiring closets. This application note provides guidelines for using the Rack Air Containment System (RACS) with these units. Additional information regarding RACS with InRow units can be found in Application Note AN-90.
135 KB
AN-66 v2 InfraStruXure Manager and Your Network
InfraStruXure Manager automatically discovers APC networked devices via a single IP address, a specified network segment, or a number of different IP address ranges up to the number of device licenses available. Since InfraStruXure Manager uses SNMP to communicate, read/write community names for individual devices must match the information in Device Access information, which is found on the System Management menu. The device user name and password must also match the Device Access information. Testing has shown that both the steady state and the discovery process increase network utilization by 0.4 to 3%. InfraStruXure Manager functions as an NTP server to managed APC devices.
286 KB
AN-35 v2 Windows Built-in Serial & USB UPS Support
Windows XP is built on Windows 2000’s reliability, but a Personal Computer is only as reliable as its AC power. APC and Microsoft have partnered to include built-in support of Uninterruptible Power Supplies (Battery Backup Systems) in the Windows XP operating system in order to prevent crashes and data corruption due to poor power quality.
467 KB
AN-115 v0 UPS Power for the InfraStruXure InRow SC
The InfraStruXure® InRow™ SC (ACSC100 and ACSC101) is a self-contained air conditioner for server rooms and wiring closets. This application note outlines considerations for powering the unit from a UPS.
54 KB
AN-48 v2 Ventilation and Cooling Requirements for the Symmetra PX UPS
Data centers requires proper ventilation to remove the heat generated by its equipment and provide sufficient air quality. The Symmetra PX UPS supports up to 40kW of equipment. This large amount of power supported and its ventilation requirements are sufficient to remove the heat generated by the UPS, keep the batteries at their ideal temperature, and remove any hydrogen generated. Data centers are an excellent location for Symmetra PX UPS solutions.
53 KB
AN-113 v0 Configuration Types and Sequence of Operations for the InfraStruXure InRow SC
The InfraStruXure® InRow™ SC (ACSC100 and ACSC101) is a self-contained air conditioner for server rooms and wiring closets. This application note outlines various operating modes and the impact of user configurable setting on unit component behavior.
140 KB
AN-103 v1 How InfraStruXure® Central Server v5.x Relates to Your Network
This Application Note explains how InfraStruXure Central Server v5.x relates to your network, provides information on the discovery process and other network-based functionality, and how the operations relate to your network.
220 KB
AN-135 v1 InfraStruXure Central Surveillance: Performance Tuning and Remote Storage
Due to the amount of data that is generated by InfraStruXure Central Surveillance, it can be very important to properly plan your Surveillance deployments. You can use the information included in this document to determine approximately how much data will be generated by your surveillance-licensed appliances and to performance tune your appliance cameras to minimize their impact on your network. This document also provides information on how you can configure your appliance to use network attached storage (NAS) to store surveillance data remotely until it is needed by InfraStruXure Central, thereby minimizing network traffic and optimizing the efficiency of your InfraStruXure Central deployment.
433 KB
AN-67 v1 APC Network Management Card Security Implementation
This document highlights the security implementation on the APC Network Management Card, and should be used as a high-level overview of the Network Management Card functionality.
563 KB
AN-69 v1 Rack Air Distribution Unit
Detailed description how to apply the various uses of the Rack Air Distribution Unit into a datacenter or IT space.
135 KB
AN-70 v2 InfraStruXure Manager Appliance v4.x Building Management System Integration
This application note explains the integration of APC’s InfraStruXure Manager Server Appliance v4.x with a building management system (BMS).
362 KB
AN-134 v1 Using Sealevel Systems Equipment with APC NetBotz Appliances
Sealevel Systems provides innovative hardware products that can enable additional connectivity and control of I/O devices that they are interfaced with. Using the manageability and flexibility of NetBotz products, a wide array of I/O devices can be managed, monitored, and controlled. Through the combination of these two elements, a robust and flexible, managed network of I/O devices emerges. This document provides the information necessary to create an environment using the Sealevel and NetBotz equipment.
172 KB
AN-104 v1 InfraStruXure® Central Server v5.x: Security
This Application Note explains the security associated with APC InfraStruXure Central Server v5.x, providing details on the various security layers within APC InfraStruXure Central as well as discussing the built-in firewall, access levels, and various network ports.
226 KB
AN-112 v0 Best Practices for Deploying the InfraStruXure InRow SC
The InfraStruXure® InRow™ SC (ACSC100 and ACSC101) is a self-contained air conditioner for server rooms and wiring closets. This application note outlines best practices to be used when deploying the units in these IT spaces.
233 KB
AN-105 v2 Monitoring Third-Party Devices with APC NetBotz Appliances and InfraStruXure Central
This Application Note details the variety of third-party devices that can be monitored with APC Security and Environmental Monitoring Appliances and InfraStruXure Central.
50 KB
AN-96 v0 Rack Air Removal Unit SX Application Guidelines
The Rack Air Removal Unit SX (ARU SX) is a rack mounted fan system for use with NetShelter enclosures. This application note outlines various considerations for applying the ARU SX
973 KB
AN-97 v0 Graceful Unattended Shutdown Solutions for Single, Dual- and Triple-Corded Servers
This paper describes how the UPS Network Management Card and PowerChute Network Shutdown works under various shutdown scenarios based on the number of UPSs and number of server power cords involved. Also discussed is a scenario describing how to handle server shutdown in APC InfraStruXure for medium data centers.
1081 KB
AN-152 v0 APC Virtual Media: Stay in Your Chair, Stay in Control
To ensure non-stop delivery of essential business services to users across and beyond the enterprise, data centers require constant, diligent server administration. Virtual Media (VM) addresses the issues of operational efficiency and security by allowing servers to access storage media anywhere across the enterprise. This Application Note covers a basic scenario of mapping a remote CD and image. You will understand which APC products are required as well as the steps involved to ensure systems meet the base requirements for supporting Virtual Media, mapping physical storage and displaying related statistics.
1457 KB
AN-98 v0 Using PowerChute® Network Shutdown in a Redundant UPS Configuration
This application note explains the graceful unattended shutdown process for servers connected to UPSs in a redundant configuration.
651 KB
AN-146 v1 Hot Aisle Containment Application Guidelines and Approved Configurations
The Hot Aisle Containment System (HACS) is a modular ceiling panel and door system for use in isolating the supply and return air between an APC NetShelter rack and an APC InRow® cooling solution. The containment system is designed to create a separate environment for air distribution in order to prevent mixing of hot and cold air streams, resulting in a more predictable cooling pattern. The modular design and ability to retrofit to an existing Netshelter rack enables medium to high density racks to be cooled in an autonomous environment without overcooling the room.
261 KB
AN-117 v0 PEX-AL-PEX Application
APC uses Cross-linked Polyethylene piping as a reliable choice for distribution of water and glycol based cooling fluids through the InfraStruXure® Cooling Distribution Unit (CDU). Its construction allows flexible installation techniques that minimize joint use and prevent vibration transmission, while providing good strength and durability for system pressures under 1.03 MPa (150 psig). This paper will explain how Polyethylene pipe is made, its construction, uses, safety ratings, and design constraints associated with the material.
241 KB
AN-46 v1 Distributed Generator System Synchronization
Distributed Generator Synchronization can be utilized when using a Delta Conversion UPS in a distributed-redundant UPS design. The scope of this paper is to cover generator synchronization in a distributed generation system for critical power applications. Distributed generation is commonly used with distributed redundant Uninterruptible Power Supply (UPS) designs. Generator synchronization can be used in this UPS system design to achieve up-stream synchronization to improve availability with Delta Conversion Technology UPS systems.
596 KB
AN-90 v2 Rack Air Containment Application Guidelines and Approved Configurations
The Rack Air Containment System (RACS) is a modular front and rear plenum for use in isolating the supply and return air between an APC Netshelter SX rack enclosure and an APC InRow™ cooling solution. The containment system is designed to create a separate environment for air distribution in order to prevent mixing of hot and cold air streams, resulting in a more predictable cooling pattern. The modular design and ability to retrofit to an existing Netshelter SX rack enables medium to high density racks to be cooled in an autonomous environment without overcooling the room mixed with lower density loads.
155 KB
AN-82 v1 Redundant Group Control for FM or IR units
Redundant Group Control for FM and IR is a collection of two, three or four systems that provide redundant functionality, runtime balancing, prevention of demand fighting, load sharing and backflow prevention
178 KB
AN-139 v0 The Advantages of the APC UPSync(tm) Module
This application note discusses the fundamental concepts of the UPSync™ system. Many common misconceptions promoted by competitors about APC’s ability to synchronize UPS modules are dispelled. The subjects of 2N power distribution systems and power system synchronization are addressed. The various myths are described and criticized. The advantages of the APC design to the end-user or system designer are discussed.
202 KB
AN-25 v1 Installation of InfraStruXure For Medium Data Centers with an Emergency Power Off Circuit
Many installations require the use of and Emergency Power Off (EPO) circuit to disconnect power from a room or apparatus. This requirement was taken into consideration during the design of the APC InfraStruXure architecture.
1070 KB
AN-160 v0 NetBotz Building Management System (BMS) Integration
The Modbus protocol is a standard in the industry and is supported by almost all of the BMS vendors. APC integrates Modbus TCP over an Ethernet connection and Modbus RTU/ASCII over a serial connection for NetBotz® communication with a BMS (e.g. T.A.C Continuum™ and Vista™, Johnson Controls’ Metasys™, Siemens’ APOGEE™, ALC’s WebCTRL™, etc.). This paper explains the integration of the APC NetBotz® appliance v3.2 release with a Building Management System.
829 KB
AN-61 v0 Installation of InfraStruXure For Large Data Centers with an Emergency Power Off Circuit
Many installations require the use of and Emergency Power Off (EPO) circuit to disconnect power from a room or apparatus. This requirement was taken into consideration during the design of the APC InfraStruXure architecture.
1031 KB
AN-91 v1 Alternative Network Connectivity Options for APC NetBotz Monitoring Appliances
APC NetBotz monitoring appliances come standard with a 10/100 Ethernet port. This is the predominant connection for most customers, however for some locations customers may require a different network connection type. Or, the customer may desire a backup communication link in the event the Ethernet connection is lost.
163 KB
AN-156 v0 InfraStruXure Central v5.1 Building Management System Integration
Provide a technical description of how InfraStruXure Central can integrate into a higher level building management system through the ModBus TCP protocol
249 KB
AN-159 v0 Hot Aisle Containment System (HACS) and Data Center Fire Protection
The design of data centers around Hot Aisle Containment Systems (HACS) is growing in popularity. Engineers and, increasingly, Authorities Having Jurisdiction (AHJ) are questioning the need for fire protection in the hot aisle; specifically: incipient stage fire detection (high sensitivity smoke detection), smoke detection, fire suppression, sprinkler protection. This application note describes fire protection strategies for hot aisle containment systems. It is intended to clarify questions regarding detection and suppression requirements as applied to asset protection as well as address misconceptions within the HACS space.
186 KB
AN-62 v2 Dedicated Dehumidification Cycle for CRAC
This application note discusses how the NetworkAIR FM dedicated dehumidification works and saves on the reheat and humidification requirement.
204 KB
AN-74 v1 Configuration of InfraStruXure for Data Centers to Support Dell PowerEdge 1855 Blade Servers
The Introdcution of blade servers has created many challenges for those who design and support NCPI. InfraStruXure for Data Centers can be configured to meet the dynamic needs of Dell PowerEdge 1855 Blade Servers
297 KB
AN-157 v0 InfraStruXure Central Web Services Integration
This will describe how InfraStruXure Central will integrate with higher level management tools through a Web Services API
388 KB
AN-73 v1 InfraStruXure Manager Server Appliance v4.x and PowerChute Network Shutdown
Explains how to gracefully shut down servers using PowerChute Network Shutdown and the UPS Network Management Card as well as monitor the UPS through APC's InfraStruXure Manager 4.x
231 KB
AN-79 v1 NetworkAIR FM and IR Customer Interface Input/Output Modules
Each NetworkAIR FM and IR unit is supplied with one Programmable Customer Input/Output Module (PCIOM) as a standard configuration and up to three more modules can be added to each unit if required.
68 KB
AN-56 v2 Real time monitoring and control of suction pressure for the NetworkAIR FM
Describes the control scheme for monitoring and controlling suction pressure in the NetworkAIR FM. Head pressure control prevents freezing of the cooling coil and facilitates stable heat removal and efficiency.
63 KB
AN-59 v1 NetworkAIR FM PID Tuning
This application note describes a procedure for tuning the Proportional/Integral/Derivative (PID) control loops utilized in the FM Series Computer Room Air Conditioner (CRAC). The FM Series CRAC employs PID control loops for: Cooling; in Multi-Cool, ECON and Chilled Water only configurations. Dehumidification; in Multi-Cool and Chilled Water only configurations. Reheating; in systems equipped with electric reheaters.
216 KB