Technical FAQs

Ask a Question

Video: How do I Configure the Date/Time, NTP Server, and Regional Settings on Data Center Expert?

Issue:
How do I Configure the Date/Time, NTP Server, and Regional Settings on Data Center Expert?‚Äč

Product Line:
StruxureWare Data Center Expert (DCE)

Cause: 
To ensure that data is stored and retrieved properly, ensure that DCE has a current date/time defined.  You can also set DCE as NTP server so that devices that are configured for NTP can be set to pull their Date/Time from DCE.

Resolution:



1) Open the DCE client and navigate to the System Menu > Server Administration Settings > Time Settings.

2) Under the Date and Time section, the current Date and Time that is set on the server is displayed.  If this is incorrect, you can select Use Client Time to use the current computers time that you are using the client on.  When you change the date/time, the appliance requires a reboot.




3) You can enable DCE to act as an NTP server to provide date/time to your devices that are configured with DCE as their NTP server.  You can set the time manually or choose for DCE to get its Date/Time from a Remote NTP server.




4) You can change your Regional Settings for the DCE Appliance, including server locale, 24-hour clock, and server time zone.

Was this helpful?
What can we do to improve the information ?