Technical FAQs

Ask a Question

Video: How to change the temperature thresholds on a Network Air FM unit

Issue:
How to change the temperature thresholds on a Network Air FM unit
 
Product line:
FM35-50, ACFM, IR40
 
Environment:
All Serial Numbers
 
Cause:
Install Operation
 
Resolution:
 


How to change the temperature thresholds on a Network Air FM unit follow the below procedures
 
1 Press ESC until you reach the main menu (On/Off)
 
2 Scroll to SETUP and press ENTER
 
3 Scroll to SYSTEM 1 and press ENTER
 
4 Press ENTER on ALARMS.
 
5 Press ENTER on TEMPERATURE THRSHLD
 
6 Select which threshold you want to change and then press ENTER.
 
7 Use the UP or DOWN arrows to select the desired temperature.
 
8 Press ENTER when finished
 
9 Press ESC until you get back to the status screen
 
Was this helpful?
What can we do to improve the information ?