Can a full height 0U PDU be installed into the NetShelter SX Colocation cabinet?
Issue:
Some customers may want to mount a full height 0U PDU into the NetShelter SX Colocation cabinet.
Product Line:
NetShelter SX Colocation
Environment:
All versions and serial ranges.
Cause:
Customers may want to use a PDU other than those recommended for use in the cabinet.
Resolution:
The NetShelter Colocation cabinet does not support the use of a 0U PDU. For a full list of the PDUs that are compatible with the Colocation cabinet please see the NetShelter Compatibility Chart in Knowledge Base document FA158651.