If the required hardware has been misplaced, the following parts will need to be ordered. Please note that the bolts and washers are not something regularly stocked in our warehouses. The bolts, split washers, and flat washers can be purchased at a local hardware store.
(4) 870-6273A - L-bracket used to anchor Symmetra LX to floor
(8) 812-0011A - 5/16" 18 thread count x1" long Bolts used to attach L-bracket to pallet support brackets
(8) 812-0012A - 5/16" Flat washers to be used with 812-0011.
(8) 812-0014A - 5/16" Split washers to be used with 812-0011.
NOTE: If the UPS was originally a rack-mount system and was converted to a tower form factor, the following parts will be needed in addition to the parts listed above.
(2) 870-6272 - Pallet Support Bracket
(18) 810-2003 - 10-32 Nut to attach Pallet Support Brackets to chassis