Technical FAQs
Technical FAQs
Cause
v6.0.6 and higher AOS versions contain new user types defined by permissions. This article is intended to highlight each and define their respective permissions.
If you upgrade your NMC2 firmware from v5.1.X to v6.X.X, as noted in knowledge base article ID FA167693, your 5.1.X users (administrator, device, read-only) will transfer over to v6.X.X.
Along with new user types, multiple users of each type can be created and logged in to the NMC2 at the same time.
Resolution
Refer to the information below. regarding the types of users that can be created.