Technical FAQs

Ask a Question

What communications cable is needed with my Smart-UPS and PowerChute Business Edition?


Issue:
What communications cable is needed with my Smart-UPS and PowerChute Business Edition?

Product Line:
Smart-UPS and PowerChute Business Edition (PCBE)

Environment:

UPS Model Part Number of Communications Cable
SURTD, SMX, SMT, SMC* 940-0117B or 940-0273A (USB)
940-0625A or 940-1525A (smart signalling)
940-0128D (simple signalling)
SUA, SU, Other Smart-UPS 940-0024 (smart signalling)
Any USB-compatible Smart-UPS Any standard USB cable
8-Port UPS Interface Expander 940-0020 (basic port connection)
940-0024 (advanced port connection)
Interface Expander Card 940-0020 (simple signalling)

NOTES: 
* SMC model UPS do not ship with serial communications cable. SMC model UPS ship with USB cable only.

Was this helpful?
What can we do to improve the information ?