Standard Lens Specifications for the WallBotz 500 & Camera Pod 120
Issue:
Standard Lens Specifications for the WallBotz 500 & Camera Pod 120
Product Line:
NetBotz
Environment:
NetBotz 500 / Camera pod 120 (Owl 1 pod only)
Cause:
Lens specifications.
Resolution:
Lens Specifications for the standard lens on the WallBotz 500 / Camera Pod 120 (Owl 1 pods only)
Manufacturer: Marshall Electronics
Model: V-4508
Size: 1/2 inch format
Focal Length: 8mm
Note: The focal length distance between the lens and the imager. F-Stop: 1.3
Note: The f-stop affects depth of field, or how much is in focus in front of and behind the subject.
Field of View (horizontal x vertical in degrees): 40x28