Technical FAQs
Technical FAQs
Issue
How can I extend the cable length of a Symmetra LX or Symmetra RM XR battery frame?
Product Line
Symmetra LX
Environment
All serial ranges
Cause
The need may arise for there to be space between the UPS mainframe and XR frames i.e. if they cannot be installed in the same rack or enclosure.
Resolution
There are two kits that would allow you to extend the length of a Symmetra RM or Symmetra LX extended run frame cable.
SYOPT4: 4ft (1.2m) Extension Cable
SYAOPT5: 15ft (4.6m) Extension Cable
Please Note: These cables are NOT compatible with the legacy SYXR4 and SYXR12 Extended Run cabinets designed for use with Symmetra Power Array.