Technical FAQs

Ask a Question

Data Center Expert | Why do I not see certain menu options in the desktop client?

When logging in to the Data Center Expert client, certain menu options are not available, such as particular items from the “System” menu.

Product Line:
StruxureWare Data Center Expert (DCE)

Struxureware Data Center Expert (all versions)

The user is configured to have restricted access to the StruxureWare Data Center Expert appliance.


Contact the administrator for the DCE server to grant additional rights to your DCE account.
Was this helpful?
What can we do to improve the information ?