Technical FAQs

Ask a Question

Video: How to change the alarm delays on a Network Air FM unit

Issue:
How to change the alarm delays on a Network Air FM unit
 
Product line:
FM 35-50, IR40, ACFM400, ACFM200
 
Environment:
All Serial Numbers
 
Cause:
Install, Configuration
 
Resolution:
 


To change the alarm delays for temperature and humidity through the front display:
  1. Press ESC key until you get to the main menu.
  2. Then select SETUP and then SYSTEM 1.
  3. Select ALARM and then select ALARM DELAYS.
  4. Now you have a choice of either Temperature or Humidity. Select one by using the UP or DOWN arrows.
  5. Then press ENTER and now you can change the delays times anywhere from 0-999 seconds.
 
 
Was this helpful?
What can we do to improve the information ?