Technical FAQs

Ask a Question

How do I configure my Call UPS SmartSlot Card (AP9608)?



Issue

How do I configure my Call UPS SmartSlot Card (AP9608)?


Product Line
  • UPS Device Management
    • Call UPS - AP9608 (discontinued)


Environment

  • All serial numbers
  • All installation scenarios


Cause

General configuration information



Resolution



1.) Install the Call-UPS into the Smart-UPS, Matrix-UPS, Symmetra, or other supported UPS.

2.) Attach the null modem cable (APC part # 940-0103) from the AP9608 Management Port to a serial communications port on a computer with a terminal emulation program available.


Please note that if you have the scroll lock on, HyperTerminal or similar will not communicate properly with an APC UPS or accessory.

3.) Establish a terminal emulation session at the following settings: 9600 baud, 8 data bits, 1 stop bit, no parity. Many terminal packages are available and will function as long as these parameters are selected.

4.) Major characteristics to configure:

Set Answer Rings = 1 or 2, set baud rate to one that is supported by attached modem.
 
5.) Fully close out of Call-UPS II configuration screen by pressing the <Esc> key as many times as needed.

6.) Remove null modem cable and attach modem's communications cable to the Call-UPS II Management Port.

 
 
Was this helpful?
What can we do to improve the information ?