Server Access options are blank on StruxureWare DCE Desktop Client after upgrade to v7.5.0
Issue:
Server Access options are not visible after upgrading to v7.5.0
Product Line:
StruxureWare Data Center Expert
Environment:
Version 7.5.0
Cause:
It has been seen that after upgrading systems to v7.5.0, the Server Access options are blank if HTTP had been disabled prior to the upgrade.
Resolution:
In order for this to be corrected, you must contact your local Technical Support for StruxureWare Data Center Expert. A remote session may be required to resolve this issue. In the meantime, if you have a recent backup from prior to the upgrade, you may want to restore that backup to the server.