Technical FAQs

Ask a Question

Are the NetShelter SX Networking cabinets available in a Shock Package version?

Issue:
None of the Networking cabinets have Shock Package versions.

Product Line:
NetShelter Networking

Environment:
All versions and serial ranges.

Cause:
Customers may want to ship the Networking cabinets with equipment installed.

Resolution:
No, the NetShelter SX Networking cabinets are not available in Shock Package versions. The NetShelter Networking cabinets have mounting rails that are open to allow greater airflow. This design has not been tested for shock packaging.
Was this helpful?
What can we do to improve the information ?