Technical FAQs

Ask a Question

Can a full height 0U PDU be installed into the NetShelter SX Colocation cabinet?

Issue:
Some customers may want to mount a full height 0U PDU into the NetShelter SX Colocation cabinet.

Product Line:
NetShelter SX Colocation

Environment:
All versions and serial ranges.

Cause:
Customers may want to use a PDU other than those recommended for use in the cabinet.

Resolution:
The NetShelter Colocation cabinet does not support the use of a 0U PDU. For a full list of the PDUs that are compatible with the Colocation cabinet please see the NetShelter Compatibility Chart in Knowledge Base document FA158651.
 
Was this helpful?
What can we do to improve the information ?