Where can I find the NetBotz Advanced View installer?
Issue:
Where can I find the NetBotz Advanced View installer? Product line:
NetBotz Environment:
NetBotz version 2 and 3 Advanced View Cause:
To be able to configure a NetBotz appliance Advanced View is required.
Resolution:
Advanced View can be obtained in two locations
Advanced View installer is located on the CD that is bundled in the documentation package that is boxed with the unit.
If the CD is misplaced, Advanced View installer can also be found on the web.
For the most recent version of Advanced View can be found at http://updates.apc.com/botz/av/install.htm
For older versions of Version 3 NetBotz appliances, Advanced view is contained in the NetBotz firmware download file found on http://www.apcc.com/tools/download or the product page.
For NetBotz version 2 appliances (320, 420, and 500) Advanced View version 2.6.2 can be found here:
http://updates.netbotz.com/releases_500/2.6/install.htm
Please note that it is recommended that you match the version of Advanced View with the version of Botzware on the appliance. Failure to do so may cause unsuspected results and errors.
Also note that Advanced View 2.6.x has not been tested on Windows 7 or higher and may not appear correctly