Technical FAQs
Technical FAQs
Issue
The StruxureWare Data Center Expert client cannot launch to devices on the private LAN when it is installed on Linux with the network proxy configured.
Product Line
StruxureWare Data Center Expert
Environment
StruxureWare Data Center Expert user interface (any version)
Linux
Cause
Linux private device launch does not work if the DCE Linux Client has a network proxy enabled.
Resolution
Add the DCE server IP address to the Linux client network proxy ignore list, or disable the proxy.