Technical FAQs

Ask a Question

How to Install a OROA or A LAC Valve as part of a Flooded Receiver Package

Issue:  
How to Install a OROA or A LAC Valve as part of a Flooded Receiver Package

Product line:
ACRD1XX, ACRD2XX, ACRP1XX, ACRD5XX, Uniflair DX, Network Air FM, InRoom DX

Environment:  
All Serial Numbers

Cause:  
Install

Resolution:
The installation of the valve requires the proper alignment.

 

Please reference the diagram below

 

C= Line from the bottom header of the condenser

 

R=Line from the valve to the Flooded Receiver

 

D=Discharge line from the Compressor

 










 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Was this helpful?
What can we do to improve the information ?