Technical FAQs

Ask a Question

Will the NetShelter CX fit through standard doors?

Issue:
Will the CX fit through a standard door opening?

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
Need to ensure the NetShelter CX will fit up the stairs, into the elevator or through a doorway.
 
Resolution: 
All the units, including the 38U, are designed to go through a standard doorway. They measure 750 mm /29.5” wide x max 1950mm/76.7” tall.
 
Was this helpful?
What can we do to improve the information ?