Technical FAQs
Technical FAQs
Issue
XR frame displays E1 or EF. The mainframe indicates that an XR frame fault exists.
Product Line
Symmetra Power Array
Symmetra RM
Symmetra LX
Single Phase Symmetra XR Frames
Environment
All serial ranges
Cause
This error indicates that the XR communication card (either SYXRCC or SYAFSU16) located in the XR frame has experienced an internal problem.
Resolution
The card will need to be reseated. If reseating does not clear the fault, the card must be replaced.