Technical FAQs

Ask a Question

What is the power factor (PF) of the ACSC cooling unit?

Issue:
What is the power factor (PF) of the ACSC cooling unit? 
 
Product line:
ACSC100, ACSC101
 
Environment:
InRow Cooling
 
Cause:
 
Resolution:
Most of the PF comes from the compressors. The unit fan power bus rectifiers are PF corrected.
ACSC100 – 0.98
ACSC101 – 0.98
Was this helpful?
What can we do to improve the information ?