Can I use multiple ACSC1XX units in a single room?
Issue:
Can I use multiple ACSC1XX units in a single room?
Product line:
ACSC1XX
Environment:
All Serial Numbers
Cause:
FAQ Resolution:
Yes, the only limitation is the ability of the ceiling plenum to handle the airflow and heat rejection from the SC units. The SC units now have group controls built into the firmware that allows them to talk to one another.