Technical FAQs

Ask a Question

What does “equivalent pipe length” mean?

Issue:
What does “equivalent pipe length” mean?

Product line:
All Cooling Units

Environment:
All versions.

Cause:
Install

Resolution:
Equivalent pipe length, EPL is a calculated numeric value that converts the friction losses assoc with valves, bends, fittings and fluid velocities to a representative length of straight pipe of a stated type (metal, plastic, etc) and diameter.

 

 
Was this helpful?
What can we do to improve the information ?