Technical FAQs

Ask a Question

Devices Will Not Be Discovered If Timeout is Longer Than 60 Seconds in ISX Central

Issue:

Devices Will Not Be Discovered If Timeout is Longer Than 60 Seconds in ISX Central

Product Line:

StruxureWare Central / Data Center Expert

Environment:

StruxureWare Central / Data Center Expert version 7.0 and earlier.

Cause:

TIncorrect documentation.

Resolution:

If the SNMP timeout value is more than 60 seconds, the InfraStruXure Central server will fail to discover devices, even if the timeout and retry values are reduced.

The discovery entry must be deleted and a new one created in order for the devices to be discovered.

This should no longer be an issue with the release of StruxureWare Central 7.2.x.

Was this helpful?
What can we do to improve the information ?