Technical FAQs

Ask a Question

Camera flicker filter not available in Netbotz advanced view with some cameras.

Issue:

Camera flicker filter not available in Netbotz advanced view with some cameras.

Product Line:

NetBotz

Environment:

NetBotz version 2 and 3 cameras

Cause:

Older version 2 camera pod 150 units had the flicker filter option under the camera configuration capture option. Newer camera pod 150 units with a revision of A2 will not show this option.

Resolution:

These cameras can be identified in the Advanced View by going to the about tab and looking for the revision. A camera pod with a revision with A0 should show this option. The version 3 camera pod CP160 will also not have this option available.

Was this helpful?
What can we do to improve the information ?