Java/Fatal Exception Error when logging into Netbotz Central as a user
Issue:
Java/Fatal Exception Error when logging into Netbotz Central as a user
Product Line:
NetBotz Central
Environment:
NetBotz Central any version
Cause:
User rights.
Since the error is related to the user interface, the log showing the error is stored locally in the Documents and Settings folder of the Logged-in user account.
i.e. $home/.netbotz/logs/nbc.txt.
Resolution:
The account they are logging in with or the NBC admin account needs to add the 'license service' read-only access to that user’s permission.