Technical FAQs

Ask a Question

FM40 AC Coil Temperature via ISX Central


The following OID will request information about FM40 AC Coil Temperature:

It is recommended to pull this OID from the unit that is selected for priority scanning by adding it as a supplemental OID. To do so please go into context menu and select :

Settings - SNMP Device Settings - Supplemental OIDs.

Was this helpful?
What can we do to improve the information ?