Technical FAQs

Ask a Question

What ACSC unit functions can I control through the web card?

Issue:
What ACSC unit functions can I control through the web card?
 
Product line:
ACSC100, ACSC101
 
Environment:
InRow Cooling
 
Cause:
 
Resolution:
Unit configuration (operating mode, capacity control, idle on leak)
Temperature set points
Unit delays
Fan speed preference
Alarm thresholds
Configure alarm output
Configure normal state of contacts
Assign service intervals
Reset component run hours
Display units (metric or English)
Was this helpful?
What can we do to improve the information ?