Technical FAQs
Technical FAQs
BotzWare for Version 1 Appliances:
Version 1.3.10 of the NetBotz Advanced View and NetBotz Firmware for Version 1 Appliances (Models 300, 300B, 310, 400) is being updated to handle the DST changes. This update incorporated changes in the firmware for the appliances as well as a patched JRE (Java Runtime Environment) for the Advanced View.
BotzWare for Version 2 Appliances:
Version 2.6.1 of the NetBotz Advanced View and NetBotz Firmware for Version 2 Appliances (Models 320, 420, 500) is being updated to handle the DST changes. The only change for the DST issue is a patched JRE for the Advanced View. However there are additional updates/fixes in BotzWare 2.6.1 that will be released as well.
Netbotz Central / ISX Central:
Version 2.5x of Netbotz Central will be updated to a version 2.5.2 for both the Central server as well as it's Console software. ISX Central 3.X does not have an issue with the change in DST
(1) Information courtesy of Sun Microsystems; http://java.sun.com/developer/technicalArticles/Intl/USDST/