Technical FAQs

Ask a Question

Newly attached camera pod on a version 3 Netbotz appliance does not show time stamp.

Issue:

Newly attached camera pod on a version 3 Netbotz appliance does not show time stamp.

Product Line:

NetBotz version 3 devices

Environment:

NetBotz "botzware" earlier than 3.3

Cause:

Not a default configuration.

Resolution:

The time stamp does not automatically appear on the image on a version 3 Netbotz appliance if a camera pod is added while the appliance is running. The time stamp will appear if the camera pod is attached when the bot is rebooted or if the pod is attached prior to booting the appliance. This happens to both the newer camera pod 160 as well as the older version 2 camera pod 120. This is addressed in Botzware version 3.3

Was this helpful?
What can we do to improve the information ?