Details Returned from MGE Devices via Netbotz Advanced Device Crawlers
Issue:
Details Returned from MGE Devices via Netbotz Advanced Device Crawlers
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for MGE systems assuming the MGE DDF (Device Definition File) is installed on the NetBotz appliance and the MGE system is SNMP enabled. Please note that not all information listed below is available on all MGE models