Technical FAQs

Ask a Question

Why can I not install PowerChute Business Edition on RHEL 5.11?


When installing PowerChute Business Edition on RHEL 5.11, the following error message is seen, “RSA/SHA1 signature:BAD, RPM cannot be installed” and the installation is unsuccessful. This happens because RPM signing keys are not supported for RHEL 5.11.


PowerChute Business Edition v9.5


RHEL 5.11


Execute the following command:
rpm --nosignature -i pbeagent-9.5.0-301.XX.rpm

NOTE: The above command will differ for 32-bit and 64-but Linux operating systems.
32-bit Linux: rpm pbeagent-9.5.0-301.i386.rpm
64-bit Linux: rpm pbeagent-9.5.0-301.x86_64.rpm

This tells RPM to ignore the signature when installing PowerChute Business Edition and will treat the RPM as unsigned.

NOTE: You will not be able to verify the RPM package on RHEL 5.11. However, this is the case for previous versions of PowerChute that were unsigned.
To uninstall PowerChute Business Edition on RHEL 5.11, execute the following command:
            rpm --nosignature -e pbeagent

Was this helpful?
What can we do to improve the information ?