If a NetShelter CX is scratched or dented can it be repaired? What color is the finish?
Issue:
A customer may want to touch up or repair damage to a NetShelter CX cabinet.
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
A NetShelter CX cabinet has been scratched or damaged.
Resolution:
There are a couple of options a customer can use to disguise damage, but at closer inspection any repair work will remain visible. In most cases the repair will be visible.
A color marker can help cover a scratch. To fill a hole or indentation it may be necessary to first fill it, then paint it.
These are the colors that will patch:
RAL - 7016
NCS - S8000-N
Pantone - 433U