Technical FAQs

Ask a Question

Do the NetShelter SX Shock Packaging cabinets include the AR7701-S mounting bracket?

Issue:
Customer wants to know if the pallet brackets from the Shock Packaging can be used to mount the cabinet to the floor.

Product Line:
NetShelter SX Shock Package

Environment:
All versions and serial ranges.

Cause:
Customer purchased a Shock Package cabinet: AR3xxxSP.

Resolution:
The pallet brackets of the Shock Package cabinets can not be used in seismic installations. For seismic installations please use AR7701-S.
The Shock Package cabinets do not include the AR7701-S mounting bracket. It must be purchased separately.
Was this helpful?
What can we do to improve the information ?