Technical FAQs

Ask a Question

Disconnecting and Reconnecting a Configured RS232-Based Sensor or Output Control Device Can Cause Device Settings to be Lost

Issue:

Disconnecting and Reconnecting a Configured RS232-Based Sensor or Output Control Device Can Cause Device Settings to be Lost

Product Line:

NetBotz

Environment:

NetBotz and RS232 sensor connections

Cause:

Settings associated with RS232-based sensors or output control devices may not be preserved if the device is disconnected and then reconnected.

Resolution:

Once you have connected and configured settings for an RS232-based sensor or device, do not disconnect or relocate this device unless you are prepared to reconfigure the device.

Was this helpful?
What can we do to improve the information ?