Technical FAQs

Ask a Question

Cannot Restore an ISX Central Backup when a user has special characters in the login account password

Issue:
Cannot Restore an ISX Central Backup when a user has special characters in the login account password

Product Line:
InfraStruxure Central

Environment:
Version 5.1

Cause:
If you create a share on a remote system to use as a repository for an ISX Central 5.1 backup and the user account used to access that share has any special characters in their password, the restore of that backup will fail

Resolution:
To resolve this issue, either use a user that has a password without special characters or create one for this specific action and remove the user or change his password until needed again. This issue was resolved in 6.x.

Was this helpful?
What can we do to improve the information ?