Technical FAQs

Ask a Question

Retrieving Picture Images from NetBotz Appliances Programmatically

Issue:

Retrieving Picture Images from NetBotz Appliances Programmatically

Product Line:

NetBotz

Environment:

NetBotz version 1, 2, and 3

Cause:

Alternative means of retrieving camera images.

Resolution:

The current image from the Version 1 Appliances can be retrieved from the following URL:

http://botip/campic.jpg

The current image for Version 2 Appliances can be retrieved from the following URL:

http://yourbotzip/images/nbOwlEnc_0_CAMERA/QVGA/campic.jpg


The Version 2 Appliances have more features however to adjust such as which camera and resolution. To change these options, simply change the following values:

nbOwlEnc_0_CAMERA
Change the 0 to a 0 1 2 or 3 to select the desired camera.


Change QVGA to one of the following to select the desired resolution.

VGA = 640x480 (VGA)
XVGA = 1280x1024
EVGA = 1024x768
SVGA = 800x600
QVGA = 320x240
QQVGA = 160x120
 
Was this helpful?
What can we do to improve the information ?