Technical FAQs

Ask a Question

NetBotz version 2 Power Control Pod Maximums

Issue:

NetBotz version 2 Power Control Pod Maximums

Product Line:

NetBotz

Environment:

NetBotz version 2

Cause:

Maximum configuration.

Resolution:

Up to 16 power control pods can be connected to a NetBotz 500

Up to 4 power control pods can be connected to a NetBotz 420 (wall or rack) 

The NetBotz 320 (wall or rack) does not support a USB connection and hence does not support any power control pods.
Was this helpful?
What can we do to improve the information ?