Technical FAQs

Ask a Question

Are APC by Schneider Electric network enabled products IPv6 compliant?


All APC by Schneider Electric Network Management Card 2 devices with AOS (APC Operating System) > version 5.1.1 or higher are Certified IPv6 Ready (Phase-2/Gold Logo) by the IPv6 forum (http://www.ipv6ready.org). The Logo ID# is 02-C-000439 and was approved on Feb 15, 2010. The Phase 2 Gold Logo verifies optimum compliance with the IPv6 protocol.

UPS Network Management Card 2 SKUs include but are not limited to: AP9630, AP9631, AP9635, AP9630CH, AP9630J, AP9631CH, AP9631J, AP9635, and AP9635CH.

Devices that have a mini embedded Network Management Card 2 or UPSs with a preinstalled Network Management Card 2 are Certified IPv6 Ready (Phase-2/Gold Logo) by the IPv6 forum (http://www.ipv6ready.org), as above. 

Devices with mini embedded Network Management Card 2 include but are not limited to: second generation APC by Schneider Electric Rack Power Distribution Units and select Audio/Video products.

You can check the model and AOS version from the interface of your Network Management Card 2 from the command line interface via telnet, SSH, and local access by issuing the about command. Via the web interface, navigate to the Administration tab->General->About to view the model and AOS version.

Additionally, certain APC by Schneider Electric KVM switches include IPv6 functionality, including AP5610, AP5615, AP5616, KVM2132P, KVM2116P, and KVM1116P.
Was this helpful?
What can we do to improve the information ?