Technical FAQs

Ask a Question

Video: How to Change the self-test Interval on your Symmetra PX 10-80KVA ups

Issue:
Configuring when the on-battery self-test runs on the Symmetra PX1 UPS via the PowerView integrated display
 
Product line:
Symmetra PX1
 
Environment:
All Product models, all serial numbers
 
Cause:
It may be necessary to change the battery test interval from the default of 14 days.

Resolution:
Select “Setup” from the Main Menu
Select ‘Other’ from the Setup menu
Select “Self-test”

Options are:
At Power On
Every 7 Days
Every 14 Days
or Disabled

Select the desired interval and hit Esc to save the change.
Your self test will now run at this interval.

The following video demonstrates this procedure:

Was this helpful?
What can we do to improve the information ?