Technical FAQs

Ask a Question

InfraStruXure Central 5.0 server hangs after incomplete Authentication Server configuration

Issue:

InfraStruXure Central 5.0 server hangs after incomplete Authentication Server configuration

Product Line:

InfraStruxure Central

Environment:

InfraStruxure Central 5.0

Cause:

This issue has been seen in a few cases where a user will click "Finish" instead of "Next" and Authentication Server configuration will not complete. With this invalid configuration, the server will fail to boot the next time it is brought back up or rebooted.

Resolution:

Version 5.1 StruxureWare Central and higher should not experience this issue.


Was this helpful?
What can we do to improve the information ?