Technical FAQs

Ask a Question

What happens when the optional installed EPO is triggered on the single phase Symmetra?

Product Line
Symmetra LX
Symmetra RM
Symmetra Power Array

Resolution
When the EPO on the single phase Symmetras is triggered it will cause the System Enable switch (on/off switch) to physically move to the "off" position. Regardless of what state the UPS is in (On battery, On line, In Bypass) the Symmetra will immediately be powered off entirely. This includes all load attached. 
Was this helpful?
What can we do to improve the information ?