PX2 100k (also apply’s to the Euro models) there is no need to attempt password reset via the PV display serial entry as with PX1. Instead have FSR or customer log into the UPS NMC go to Admin then the “Local Display” section and reset password from there.