Details Returned from Mitsubishi Devices via Advanced Device Crawlers
Issue:
Details Returned from Mitsubishi Devices via Advanced Device Crawlers
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for Mitsubishi UPS systems assuming the Mitsubishi DDF (Device Definition File) is installed on the NetBotz appliance and the Mitsubishi UPS is SNMP enabled. Please note that not all information listed below is available on all Mitsubishi UPS models.