Technical FAQs

Ask a Question

FM40 AC Coil Temperature via ISX Central

"

The following OID will request information about FM40 AC Coil Temperature:

.iso.org.dod.internet.private.enterprises.apc.products.hardware.airConditioners.airFM.airFMSystem.airFMSysStatus.airFMSysCoilFluidTempC

1.3.6.1.4.1.318.1.1.13.1.4.1.5.0

It is recommended to pull this OID from the unit that is selected for priority scanning by adding it as a supplemental OID. To do so please go into context menu and select :

Settings - SNMP Device Settings - Supplemental OIDs.

"
Was this helpful?
What can we do to improve the information ?